This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441EVM-G1A: Regarding ChemID

Part Number: BQ27441EVM-G1A
Other Parts Discussed in Thread: BQSTUDIO

We are using the BQ27441 fuel gauge and while looking through the technical reference manual, it states that the default ChemID for the BQ27441-G1A is 0x0128. I verified this through bqStudio. The technical reference also mentions also mentions a ChemID of 0x1202 is also used as the default battery profile (secton 6.4.2.3.13 Voltage at Charge Termination). Is there a difference between the two ChemID's? If I would like to use the ChemID 1202, am I able to select that option for the BQ27441 fuel gauge? 

Thanks,

William