Other Parts Discussed in Thread: TPS61291, TPS62740, TPS62745, TPS61099
Can we use two TPS62821 to step down two primary lithium batteries from 3.6V to 1.6V and then add them up to have regulated 3.2V output?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Thank you very much for the response. We had the TPS61291 evaluated last year. It won't be able to resolve the issue we have with the primary battery cells. Due to the lithium cell (open voltage ~ 3.6V) internal resistance issue (varies from a few ohm to a few 10s ohm even at new), when we need 60 mA pulses (~10ms) to read/write microsd on our device, the battery output voltage drops below 2.7V (that fails the usd memory). The boost converter doesn't help the high internal resistance + high current pulses issue.
Any other solution except to step down from two serial connected cells? Thanks.
Terry.