Other Parts Discussed in Thread: DRV8844, INA200
Hello everybody,
I have to build an efficient solenoid driver according to the following specs:
- Supply voltage: 8-28V
- Output current: 3A RMS / 6A peak
- The device must not heat up to more than 40°C above ambient
- Switching frequency: 25 kHz
- Load: Solenoid with an inductance of 30mH to 500mH (yes, milli) and a resistance of at least 4Ohm
I adapted a Tina9 simulation example of the BQ500101 to these conditions. The circuit seems to work, but I'm sceptical.
Do you think the device is really capable of driving such loads in reality?
Is it possible to use low switching frequencies like 25kHz?
I know this is not an intended application of the BQ500101, but I would like to profit of the compact and efficient design of integrated buck converters.
Most Brushed DC drivers (like DRV8844) are not capable of the required currents or produce too high power-loss...
Thanks for your replies,
Markus