Dear all,
My customer is now using TPS54383 and meet with some problem as below. Please help to check, thanks a lot.
Vin is 12V, Vout is 3.6V and 8V, and 3.6V is used to system, 8V is used for peripheral equipment. The 3.6V output is normal, but if output 8V the system will not work, and if remove 8V output will be ok.
The inductance is 22uH, the capacitance is 150uF.