Other Parts Discussed in Thread: BQSTUDIO
Hi,
I work with the bq27750. In bqStudio there are shown some registers like "Battery Status", "Operation Status" and so on.
I looked for these registers in the technical reference sluubi6. I found the register "Operation Staus A/B" in the chapter "11.2.30 AltManufacturerAccess() 0x0054 OperationStatus", but the bit sequence doesn't match.
When I read out the register 0x0054 by an µC I get the value like in bqstudio.
In chapter "12.12.1 Device Status" there is a matching bit sequence, but there is no explaination about the context to "11.2.30 AltManufacturerAccess() 0x0054 OperationStatus".
Moreover I guess that the high and low byte is inversely.
E.g. Operation Status A in bqstudio has the DSG-Bit at Bit1 in the low-Byte, but in the technical reference it is Bit 9, so in the high byte.
Can somebody explain the difference between the "OperationStatus" and the "Operation Status"?
Regards
Tino