Part Number: LM3478
Other Parts Discussed in Thread: TPS43061, LM5170
Hi
We want to compare the performance of load transient between LM3478 and TPS43061.
The datasheet of TPS43061 offers the following load transient figure but LM3478 is not.
Do you have similar data for LM3478?
Which device is better for load transient response?
Requirement:
Input : 6V to 8.4V
Output: 19V/1A
Efficiency : 90% target
Load transient : 2% - 3% target
BestRegards