This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28063A: About power factor data

Part Number: UCC28063A
Other Parts Discussed in Thread: PMP10116

Hello,

 

Regarding to the power factor on UCC28063A, my customer is asking a question.

(Question)

Do you have a data of power factor at 10 - 30% of rated output current under following conditions?

・Input(AC) : 240-264V

・Output395 V

・Output current (rated):1.14 A (450 W)

・AC frequency50 and 60 Hz

 

Regards,

Tao2199