Part Number: TIDA-00961
Hello,
I see in BOM that you have chosen - L102, L103 327uH 7840-09-0014 Nova Magnetics Inductor, Toroid, Ferrite, 327 µH, 0.065 ohm, TH Inductor, 1380x1310x880mil.
But you have calculated another value - As stated earlier, the desired efficiency is 0.99, V IN(MIN) = 160 V, DPEAK_LL = 0.42, P OUT = 1600 W and FMIN = 450 kHz, the calculated value of L1 and L2 are 14.78 µH. The value of the boost inductor was rounded off to 15 µH.
Can you say me why?
Best regards
Popov