Dear TI Team.
I am trying to set the input voltage 2.1 ~ 3.3V output voltage to 3V with TPS61070.
The TPS61070 does not have a power path, so I want to check if the output voltage is bypassed when 3.3V is input.
I would like to inquire if the above information is available.
Input : 2.1 ~ 3.3V (battery voltage)
output : 3.0V
Even if the input voltage is higher than the output voltage, check that there is no problem in use.
Thanks.