My customer is designing with the TPS23750 and they would like to know if this device supports Class 4 PD devices. The customer's PD device requires 24W and they are using 42V from the PSE (TPS23841). The TPW23841 allows currents up to 510mA and they would like to use all of this power. Judging from the data sheet, they can only get 410mA from TPS23750 which will produce only 17.2W.
Can you give me some guidance as to whether the TPS23750 is the correct part or if they should be looking at a difference device?