This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23753A: Problem with pwering up PoE PD circuit

Part Number: TPS23753A


Hello,

I am using the TPS23753A PD controller for my PD circuit, which is PoE type 1 class 1.

When applying a voltage of 48V and a current around 300mA at PWRSPARE1 and PWRSPARE2 nothing happens.

Could you please advise?

Thank you!

Amina