I'm trying to use the UVLO feature. This appears to be only accessed using the ENABLE pin. The datasheet specification for the pin reads:
VEN Enable Threshold Voltage V 1.6V typical
VENHYST Enable Voltage Hysteresis 0.6 V
However in the text of the datasheet (page 9):
The LM22676 also incorporates an input undervoltage lock-out (UVLO) feature. This prevents the regulator from turning on when the input voltage is not great enough to properly bias the internal circuitry. The rising threshold is 4.3 V (typ) while the falling threshold is 3.9 V (typ).
Why is there this discrepancy? 1.6V vs 3.9V?
Thanks in advance,
Mike