Other Parts Discussed in Thread: LMZ31710, LMZ31704, , LMZ31707
I am looking at these two modules to drive 5V input of an Atom 1.44 GHz up to 1.92 GHzGHz processor board like Lattepanda or Up board .
From what I read, the LM31707 QFN module is the lower cost and better suited for instantaneous current application.
I need to shut down the module when running on low battery, and the LM31707 QFN also has 3uA standby vs 32uA of the TOMOD-11pin module.
In this same 10x10mm QFN package, I can also go with LMZ31704 (4A) or higher LMZ31710 (10A) so it is a plus.
Am I on the right path?
Thanks,
Khoi