Hi,
As per the datasheet the buck boost with part# TPS63031 is fixed output of 3.3V .
But in few instance statements are confusing. Can you clarify the same.
1. Below application statement says "circuit for adjustable output voltage option" where is the resistor network also Put the part number under circuit for fixed one (TPS63031).
2. The graph says Vout=2.5V and other graph has Vout as 4.5V. How this voltage is achieved using the part TPS63031 which is a converter with fixed output of 3.3V.
Regards
Anuraj NK