Hi
Please let me ask the relation ship between CP_MODE bit and CHP_CON bit.
- From the description in CP_MODE bit, the battery voltage is connected to the current sources, then does it mean that the CHP_CON setting is ignored if CHP_CON select VOUT?
- In the 1.5x mode, does output voltage is regulated to 4.5V alreays? Or regulated to VDD x 1.5? And also is the CHI_CON setting is ignored?
- In automatic mode, the operation mode of group 1-6 and group 7-9 are selected separately?
Best Regards,
Satoshi / Japan Disty