Other Parts Discussed in Thread: TPS61099, TPS61021A
I am a bit confused regarding the output current capabilities of the TPS61221 boost converter. Although it could be said that it is related to all similar boost converters.
Is the maximum output current mentioned in the Figures of the datasheet only DC current or includes the amplitude of possible pulses as well?
So, can I use the TPS61211 in particular for an application with Vin=1.2V and Vout=3.3V, where the mean value of the current consumption is around 50mA but periodically short peaks of around 150mA appear?
Thanks