This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90160A: What can I use to program UCD90160A in-circuit with JTAG?

Part Number: UCD90160A
Other Parts Discussed in Thread: UCD90SEQ64EVM-650

I'll be getting prototype boards soon, with blank UCD90160A's soldered to the board. I have a header connected to all the JTAG pins of the 90160. So my questions are:

1. Can I somehow program these with my UCD90SEQ64EVM-650 board?

2. Does TI have a different board I should use to program these?

3. Is there a 3rd-party device that can utilize your programming files?

Or do I need the full Corelis tool set ($$$) that the factory will ultimately want to use?

Thanks