Other Parts Discussed in Thread: LM3550, TPS92515
Dear TI Forum,
I have 2 Eval Boards and 2 LEDs. When I connect LED- from 1st board with LED- from 2nd board then I see current only flowing through one LED and the current is double. That means if I set 700mA and should see 700mA on each LED ( not 1.4A only on one LED). Also what is strange I can measure 0.6V between LED+ and LED- without LED (open circuit), which is strange. Can be that output capacitor storage this voltage? But I can not discharge this capacitor which is also strange. Thanks for any support.
BR
Marcin