Hi, While designing a board utilising the BQ76PL455A-Q1 I can see in the data sheet that the COMML+ and COMML- should be left unconnected if not used (e.g. when only one BQ IC is used or in the base IC of the stack), however on the design considerations document it says these need to be pulled up and pulled down respectively. Which design is correct?
Thanks,
Alex