This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TPS650860EVM-116: Linux TPS650860EVM

Part Number: TPS650860EVM-116
Other Parts Discussed in Thread: USB2ANY

Tool/software: Linux

Hi,

I'm failing to use Extrenal USB2ANY HPA665 with TPS65086xEVM.

I have Linux  ubuntu 16.04,   IPGUI software version 2.5.0.3, and TPS65086xEVM,

When I using the onboard usb2any, and  IPGUI software version 2.5.0.3, works fine I can read registers. control powers register etc.

When I using external TI USB2ANY HPA665, 10 pin flat cable pluged in to J32 onboard JTAG connector and  IPGUI, trying to read register I get garbage readings.

I noticed that using IPGU about it recognize the onboard usb2any Firmware 2.7.0.0, while using IPGUI and HPA665 USB2ANY Firmware is 0.0.0.0.

open IPGUI , selected device onboard is recognized as "USB2ANY/OneDemo device 24AA926F26000B00" 

while the external USB2ANY recognize as  "MSP340-based HID Device 867A145124000E00"

Please advice

Thankls

Baruch