Other Parts Discussed in Thread: CSD85302L,
Hi,
We are evaluating using either CSD83325L or CSD85302L along with TI's BQ29700 for our single-cell lithium-polymer battery protection circuit. Our use-case is for a very low power wearable device (30mAh cell and max operating current of < 100mA). One of the important features of the battery protection circuit is over-current protection (both in the charge and discharge scenarios). In order to predict the trip-point of the current protection, it is important to understand the Rds(on) behavior of the MOSFETs.
Question: is there a resource that you can share with me (datasheet, application note, or comment) that would help me better understand how Rds(on) for these MOSFETs varies at low currents (in the 20 - 300 mA range)?
Thanks in advance for your help,
Michael