Other Parts Discussed in Thread: UCC256303, , UCC27324
HI
Currently, my client is developing 800W SIGNAGE using UCC28070, UCC256303, UC29002, UCC27324.
There is a problem with the overcurrent protection of UCC28070.
If the output load is increased from the input voltage of 90V to the interval of 1A, there is a phenomenon that the fet is damaged at about 1kW.
We have changed RIMO from 24kohm to 16kohm as an improvement.
At about 840W, the output voltage gradually dropped and the output current rose. 840W was maintained.
At the moment, the customer wants to adjust the OC standard to about 1000W as the initial input current instantaneously rises when LLC starts.
In contrast, RIMO and RPKLMT were adjusted, but 840W was maintained or the FET was dead as before.
Is there a way to improve this?
I will attach the corresponding circuit diagram.