This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40193: Power solution suggestion for Xilinx Artix 7 (XC7A200T)

Part Number: TPS40193
Other Parts Discussed in Thread: TPS54550, TPS53119, TPS54622, TPSM84824, TPS54824

HI, we are designing a product based on Xilinx Artix 7 (XC7A200T) fpga device and looking for some recommendation on power solution from TI.

Since our design is high performance, the estimated power consumption (from vivado) of the FPGA is around 10W,  which means the power supply has to be able to provide 10A output to VCCINT (fpga core voltage). I refer to some old design and the following chipsets were used. I wonder if this is still a viable approach and the most cost effective solution?

Any help and suggestion is appreciated!

Input is 5V from USB or 12V

TPS40193 (20A max) - VCCINT, VCCBRAM 1v0

TPS54550 (6A) - VCCAUX 1v8

TPS54550 (6A) - VCC0 3v3