Hi
Cusotmer has the following question regarding BQ25120A.
" I am trying to finish the design details so we can start layout of our ring main flex with the BQ25120A, but learning this part from the datasheet is very time consuming and I don't want to make a mistake.
I am trying for minimal IO to the part. The datasheet says I need to have !MR and !CD high for tReset before shutdown mode can happen. I need my device to enter this mode on its own. The diagram does not show !CD and !MR falling after shutdown mode is entered. In my system, these lines would drop as there is nothing to pull them up. I am disappointed that I have to dedicate IO pins in order to enter shipping mode through I2C. Can you confirm I absolutely have to do it this way. I2C only control is my desire."
Any way to do this through I2C.
Regards,
Todd