Hi
I read some similar question on E2E. However I couldn't get the answer what I wanted. So that , please let me ask.
Our customer are going to use this device at the following conditions;
Buck-Boost ; Iled=2.5A ; SW Freq = 450kHz ; PWM dim Freq = 20~100kHz
How much is the max duty cycle possible at Fsw=450kHz and Fpwm=100kHz?
As it mentioned at past post on E2E I read, it is recommended between 10Hz ~1000Hz. Is Fpwm=100kHz possible?
Regards,
Koji Hamamoto