Other Parts Discussed in Thread: CSD18531Q5A
Hello,
Currently we have been testing with this board.
1. We have changed two MOSFETs to CSD18531Q5A
2. Changed R11, R1 to set the output to 5V. (130K Ohm)
3. Our power supply specification: Meanwell SMPS 24V / 8.4A / 200W
We have tested with 5V, 6A load and it worked properly.
4. However what we ultimately want is 5V, 10A. But EVM board User Guide specifies that maximum is 8A.
We were wondering if the maximum 8A current output can be changed to 10A.
If it is possible, what parts should be changed to make it work?
Thank you
Regards
Kwangbok Jay Roh