Other Parts Discussed in Thread: TPS548D21
Now I use tps548d22 in miner. Input is 12Vdc output is 0.8V 40A.I want to control output using soft within 0.8V ±0.01V.How can I do it .thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi User,
TPS548D22 has selectable precision reference voltage by pin strapping. There is an internal option for 0.8008 V. Connect a 100 k resistor from BP to VSEL and connect a 22.1 k resistor from VSEL to GND for latch off OCP or a 19.1 k resistor from VSEL to GND or hiccup mode OCP. In this case you can connect RSP and RSN directly to the output without feedback resistors. See figure 18 in the datasheet.