This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: Button on BOOT pin (TS1) of BQ76930

Part Number: BQ76930

Hi all,

I would have a question regarding on the BOOT-TS1-/DISPLAY:

I want to have a button on TS1 line to wake up the BMS from SHIP to NORMAL mode(at the first boot and after auto ship). I would like to use this button to control the RSOC LEDs too (/DISPLAY).  In normally TS1 is used for the MOSFETs temperature,  (10K NTC)

It´s ok or can it cause any problem?

Best regards

Adam