This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EDLC charging from LiSoCl2 primary battery

Other Parts Discussed in Thread: TPS62740

I'm looking for suggestions on a part to regulate current to charge a 220mF EDLC from a LiSoCl2 battery. The current output of the battery can be as high as 50mA, but ideally lower, and the battery's open-circuit voltage is 3.6. I've seen the Energy Buffering for Long-Life Applications app note, which may be a possible solution, but perhaps there is something that is a little less complex. Thanks!