Hello Everyone,
I hope everyone is fine. I am trying to modify the "AN-2122 SM3320-RF-EV Reference Design" for one of my projects.
However, I have conflicting answers to the inductor size for this design.
1) One previous post about SM72442/5 says 20uH with 20A ratings.
2) The bill of materials says it is 27uH with the EFD-30 core but no current ratings are mentioned.
3) The bill of materials in application note states it is 2uH again with no current ratings.
Can anyone please comment on the exact size of the inductor used in the design?
Also, if I can use any other inductor with slightly different ratings for this design?
If yes, what should be the ideal range of inductor size that would work fine with this design?
Also, does it has to be EFD core or any other assembly would work fine?
I would highly appreciate a prompt response. Thanks in advance.