This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63024: Force PWM Mode

Part Number: TPS63024

Hello

My customer plan to use TPS65024's PFM/PWM pin set high for forced PWM mode.

So they have question.

Do you have data of quiescent current at 0mA in forced PWM mode.

In Datasheet, It has only PFM mode about Iq.

Regards

Taichi Nakamura

  • Hi,
    the "no-load" input current value is not specified in forced PWM mode, it depends on the operating conditions.
    However the input current in forced PWM mode can be measured on the EVM, it is in the range of 5mA at no load.