This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63031: TPS63031

Part Number: TPS63031
Other Parts Discussed in Thread: TPS63051

Dear Sirs

I like to use TPS63031 as the Picture "Typical Application Schematic" in the Datasheet.

1. If  VINA,EN and PS/SYNC is together and via  C3 on GND, did these Pins are Hi ?

2. Can I use this IC on a single side  PCB ? (Layout Example, Figure 24 in the Datasheet, but only single side pcb)

I like to use this with a Input Voltage  3 - 4.5V and fix Output 3.3V / 200mA

Many thanks for your quick answer.

Ben