This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596: w/ LM350post regulator & feedback

Anonymous
Anonymous
Part Number: LM2596
Other Parts Discussed in Thread: TL431, , LMR23630, LM76003, LMR14030, LM43603, LMR16030

I am designing a LM2596T(adjustable version) & LM350 3A buck/linear supply with input of 30V and a -15V available for use with a TL431 for output to ~0V and output ~0-24V.  A. where should I take feedback for the LM2596 and B. how should I set up the LM350 to drop ~2V  for headroom but still no more than that as it is just for a noise reduction?