Hello!
The project is implemented on the device LM3447. The input voltage is 230AC 50 Hz. Load 16DC, 300 mA (4,8 W). However, at low brightness levels of 10-20% there is a slight flicker of the LEDs with a frequency of about 5-15 Hz (visible to the eye). The project is a classical scheme. Calculations are conducted in accordance with the recommendations of the Ti. In addition, periodically a bright flash of LEDs occurs.
Regulation was made on the front and on the trailing edge of the sine. In order to prevent false triggering of the dimmer, an incandescent lamp with a capacity of 60 Watt 230 V is connected in parallel. Attempts to select Cff, Ccomp, Rac the results were not given.
What actions should I take, in order to completely eliminate the flicker of the LEDs?