This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2375: Rj45 (7499210124A) and LM2592HV

Part Number: TPS2375
Other Parts Discussed in Thread: LM2592HV

Hi

I have used 7499210124A as a RJ45 connector and I need to convert the POE voltage to 3.3 volt, so I have some questions:

1- Is it necessary to use TPS2375 or can I connect the POE voltage directly to the LM2592HV?

2- can I connect the 7499210124A RJ45 connector directly to the TPS2375 or I should use DF01S? (there is bridge rectifires in the selected RJ45)

3- is it possible to connect the TPS2375 output voltage to LM2592HV for converting POE voltage to 3.3 volt?  

Thank you in advance for guiding me