Other Parts Discussed in Thread: LM5101
Hi there,
I have built up a nice half bridge device with LM5105. Unfortunately the FETs become extremely hot and blow up after time. When I look at the switching I realize that there is no dead time at all between the signals. So I started doing some math and get a strange result.
When I enter 500kHz PWM signal at the IN Pin with 95%, the off time is only 100ns. (500kHz => 2us period * 5% => 100ns)
10k on RDT gives me 100ns dead time.
So LO should not even have the time to rise.
But when I look at the signals I see LO and HO change their level in the same moment without any dead time.
Perhaps I missed something here?
Thanks for your help in advance