This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2825: Higher frequency PUSH-PULL for GaN

Part Number: UC2825
Other Parts Discussed in Thread: LM25037

With the apparent release of GaN, SiC, higher frequency ferrites and so on, I currently using UC2825 for push-pull power supply which work with wide range VIN (DC) with stable VOUT (buck-boost sense), the switching is around 150Khz to 250KHz which I cannot go higher due to MOSFET losses. The benefits of higher frequency is reduced ferrite size.

I'm looking for alternative UC2825 than can work to 500-2Mhz frequency. I know UC2825 is rated to 1MHz but concerned with power dissipation when driving hard to MOSFET. 

Can you advise list of device that could replace UC2825, ideally without thermal shutdown?