This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS63070: Which values are need to written during creating custom parts of capacitors ?

Part Number: TPS63070


Tool/software: WEBENCH® Design Tools

I am designing power supply circuit using TPS63070.

My application requirements are as follows

Vin: 6V to 8.4 V

            Vout: 8 V

            Load current: 1.6 milliamps

I am following the design suggested by webench but BOM which is suggested by webench is not available so I want to simulate the design with alternate passive components. But some properties of capacitors are changing with frequency. In such case, value at which frequency has to be taken? Similarly how to decide the value of IRMS. 

For example, 

GRM32ER61C476ME15L - Recommended by webench. (But not available from our vendor).  

So I chose GRM32EC81C476KE15L as an alternative and I would like to validate it by simulation. Please help me in getting the following information about GRM32EC81C476KE15L

1) Derated Cap, 2) ESR, 3) IRMS, 4) Total derated capacitor.

Characteristic data about the passive component can be found below. 

psearch.en.murata.com/.../GRM32ER61C476ME15#.html

I am attaching webench report for reference.

3007.BuckBoost_1.6amp.pdf