Hello,
I'd like to use a bq24004 to charge a 2 cell series battery li-ion 8.4V, and power at the same time the rest of my circuit (a sensor 2mA of current, no problem about the voltage) from the battery. I have some questions :
1) Is it a problem if I connect rest of the circuit directly to the battery while it is charging ?
2) Is it a problem if instead of a circuit that draw 2mA I connect a circuit that draw 0.8-1A ?
3) Any suggestion ?
Best regards
Riccardo