What should be the values for R1, R2 & R3 for the following, while using TPS3700 window comparator,
Over Voltage Limit is = >5.6 V
Under Voltage Limit is <= 4.4V
Can anybody give me a solution.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What should be the values for R1, R2 & R3 for the following, while using TPS3700 window comparator,
Over Voltage Limit is = >5.6 V
Under Voltage Limit is <= 4.4V
Can anybody give me a solution.
Hello Saravanan,
We actually have released a tool for the TPS3700 that helps with these decisions. You can tinker with it yourself here (available on TPS3700 product page) and put in your own values. I have also calculated these resistor values and it seems like suitable values would be R1 = 2.09MΩ, R2 = 41.8KΩ, R3 = 163.8KΩ.
Thanks,
Abhinav.