I am using an LM2678SD-12 with the recommended Vishay Sprague 594D series capacitors. My input voltage is 24VDC. I have had 2 capacitors fail now over a period of months of development with this same circuit on two separate boards. One board had one of the 100uF capacitors fail on the 12V output side, where it shorted, caught on fire, melted, and fell off of the board. We reached out to Vishay with no luck. Next, we today had a 33uF capacitor fail on the 24V input side of the board. The input regulator turned off and prevented a fire, but the capacitor has a black mark on it and smells burnt, and the system had to restart. We believe we are using this regulator as specified with the recommended parts but this is twice we have had a capacitor fail. Do you have any advice or recommendations? We are using these regulators on numerous other designs (so far have not had a failure there).
Thanks,
Todd