Other Parts Discussed in Thread: LM2841
Hi,
I have a design that is powered to 3.3V from an industry standard 24V to 48V supply using the LM2842 switcher (slow option, 550kHz).
In order to improve efficiency I am considering the LMR13010A switcher. It appears to me that the latter could nearly make a drop-in replacement (minus the increased current limit, which is not needed in this application). The switching frequencies of both parts are almost the same, due to the large tolerance in the LM2842 part.
I also considered the LMR13006 with the slow option (1.1MHz) that would match the LM2841 with its fast option (1.25MHz). But then I would surely violate the minimum ON time constraint when stepping down from a full 40V to 3.3V.
Am I missing something? From your gut instinct is the LM2842/LMR13006 a reasonable pick for an every day switcher?
Thanks in advance and best regards,
Sven