Other Parts Discussed in Thread: TPS62147, TPS62150A
Hi all,
my customer is using the TPS62173DSGR in a typical configuration:
Vin = 12V
Vout = 5V
Iout_max = 300mA
with Lout = 2,2uH ; Cout = 22uF ; Rpg = 100K ; Cin = 10uF indicated as typical in the datasheet.
They are wondering how to increase efficiency when in stand-by mode, during this phase the device is sourcing Iout=13mA.
Do you have any recommendation on how to improve the system? If not with this device, do you suggest any other device that can achieve higher efficiency with those parameters?
Thanks and best regards,
Adrian