Hi, Im using the BQ76PL455A-Q1 to monitor 16 cells, Ive set the over voltage and under voltage thresholds for the VSENSE inputs and set the under voltage threshold for AUX0, I have enabled these faults on the FO_CTRL register, when reading the individual fault registers when simulating a fault the fault is found. However when using the GetFaultStat() as written into the example code a 1 is always returned no matter if a fault is present or not. Having run some tests I can see that with no fault present the voltage is at ~3.3V, it seems when a fault is triggered it falls to ~1.8V, however it seems this is not low enough to trigger the GetFaultStat() when used. Any Help would be greatly appreciated.
Thanks,
Alex