Hi,
I used figures 1,4,5,6,19 and section 6.7.2 of the CSD88599Q5DC MOSFET datasheet to estimate power loss but this number is far larger then my calculation based on TI application report SLVA504.
Knowns: VIN = 24V, DC = 50%, FSW = 20KHz, Ron = 1.7 mOhm, I = .614 Amps, Igate_rise = .820A, Igate_fall = .880A, Q_total = 43nC, Rnorm_150_degC = 1.9
Using Figures (1,4,5,6,19 and section 6.7.2): Figure 1 = .255W, Figure 4 = 1, Figure 5 = .964, Figure 6 = 1, Power = Figure 1 x Figure 4 x Figure 5 x Figure 6 = .246 Watts
Using SLVA504 equations: t_rise = Q_total / Igate_rise = 52.439 nS, t_fall = Q_total / Igate_fall = 48.864 nS, Psw_rise = 1/2 x VIN x I x t_rise x fsw = 7.727 mW, Psw_fall = 1/2 x VIN x I x t_fall x fsw = 7.201 mW, Psw = Psw_rise + Psw_fall = 15 mW, Prds = I^2 x RDS x Rnorm = 1.218 mW, P_total = Psw + Prds = 15mW + 1.218mW = 16 mW.
16mW is drastically different from .246W so I'm wondering what I'm doing wrong in my assumptions, calculations or comparisons between the two?
Thanks,
Nick