art Number: LP8556
Hi,
We have meet LP8556 BL flicker issue, as initial verify result, seems it caused by output current ripple not stable.
Even when Vin= 4.4V or 3.6V, current ripple ~15mA.
And when Vin under ~3.8V, PWM = low, Vout force raise up to Vboost_max, seems trigger OVP condition.
Is there any register setting is incorrect?
Below is our LP8556 application:
Vin=3.4~4.4V(1 series cell system), 4S3P LED, per LED forward voltage typ=5.9V. Iout = 60mA, using PWM direct control.
Register setting dump:
0x98 = 0x9f, 0x9E = 0x22, 0xA0 = 0xff, 0xA1 = 0xef, 0xA2 = 0x2f, 0xA3 = 0x2, 0xA4 = 0x72, 0xA5 = 0xf4, 0xA6 = 0x80, 0xA7 = 0xf5, 0xA9 = 0xe0,
0xAA = 0xf, 0xAB = 0x0, 0xAC = 0x0, 0xAD = 0x0, 0xAE = 0xf, 0xAF = 0x1, 0x00 = 0x0, 0x01 = 0x81, 0x02 = 0x30, 0x03 = 0x1, 0x04 = 0x0, 0x16 = 0x3f
Schematic:
Waveform:
Vin= 4.4V
CH1: Vout
CH4: LED1+LED2 Iout
Vin= 3.6V
CH1: Vout
CH4: LED1+LED2 Iout
Waveform:
Vin= 4.4V
CH1: PWM
CH4: LED1+LED2 Iout
Waveform:
Vin= 3.6V
CH1: PWM
CH4: LED1+LED2 Iout