This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCH010505S: Does DCH01X series or DCP02X series support Hot Swap?

Part Number: DCH010505S

Hi,

Does DCH01X series or DCP02X  series support Hot Swap? or Can we have other isolated power module support hot swap?

Thanks,

Walsh

  • DCH01 series does support hot swap as long as Vin is not greater than ^ V peak or 5.5V DC. It has minimum inrush current during hot swap.

    DCP02 series has higher inrush current during hot swap.   Its input power source during hot swap may be forced into current limiting, preventing the DCP02 from operating normally.

    Tom

    .