Hi Sir
How to select transform for 5Vin / 5Vout 0.3A application?
Does EVB used "750311880" can be use? enclosed file is i run webench result. is it ok?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir
How to select transform for 5Vin / 5Vout 0.3A application?
Does EVB used "750311880" can be use? enclosed file is i run webench result. is it ok?
Hi Anthony
Is it mean we can direct use EVB circuit in Vin4.5V~5V/ Vout 5V 0.3A. am i right?
Bogey
Hello Anthony,
According to the transformer (750311880 on slvu459 EVM specification , it mentioned that the DC current is 200mA rather than 300mA.(see attached)
Is it okay to use the same transformer on output 300mA@5V design ?
Sincerely,
Chin
It is ok using it for 300 mA. The DCR of the secondary is low enough and the saturation rating of the transformer is high enough support more than the 200 mA shown in the drawing. The values they put on the spec sheet are just the application the transformer was originally designed for.