This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27545-G1: bq27545-G1 Temperature() Units

Part Number: BQ27545-G1

We are communicating to the bq27545-G1 in an RRC battery pack. Our results from the Temperature() command are not coming back as we would expect. The data sheet says the units for this data are in 0.1K in Table 11 but the description paragraph says deg C. How is this data stored and read back when the command is called. We are expecting temperatures from about 25 - 60 deg C based on another external thermistor read out but are only getting values from about 27-35 deg C from the bq27545-G1.

Any ideas?

Thank you,

Ethan