This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65917EVM: TPS65917EVM damaged?

Part Number: TPS65917EVM

Hello teams, 

Previously, I created a thread with

" I have been testing TPS65917 EVM.

I powered the TPS65917EVM with 3.8V and 1~3A.

I have tested the PMIC several times and all of a sudden, I see that the power isn't going in enough.

When I set the voltage as 3.8V, range and limit of current as 3A, the voltage only goes in 1V while current goes in 3A."

As long as I checked, this EVM is damaged.

I purchased this EVM from Digi-key and would like to know if there is anyway that I can get EVM repaired or replaced?

Thank you.

Sincerely